Technical FAQs

Ask a Question

What is the operating temperature range of the Unity Quantum PLCs?

Issue:

Product LIne:

   Quantum PLCs

Environment:

Cause:

Resolution:

   0 to 60° C (32 to 140° F)
Was this helpful?
What can we do to improve the information ?