Technical FAQs

Ask a Question

What causes 'Decompression error #3' in Proworx 32?

Issue:
   When launching Proworx 32, this error is displayed.

Product LIne:
    Proworx 32

Environment:
    Windows operating system

Cause:
    Bad project in \Proworx\32\Projects folder.

Resolution:
   Move all projects in the \Proworx\32\Projects folder to another folder and move them back one at a time.  When the corrupt project is moved back in, the error will reappear.
This project is corrupt and cannot be corrected.
Was this helpful?
What can we do to improve the information ?