Technical FAQs

Ask a Question

Can any Quantum NOE be used in a Unity Project?

Title

Can any Quantum NOE be used in a Unity Project?

Issue
 
Product Line


Modicon Quantum Unity Pro

Environment
 
Cause

Resolution

Yes any Quantum NOE can be used in a Unity project. The NOE's do not have Software specific firmware like some of the various processors. It is recommended to flash the latest firmware for the specific NOE though.

Was this helpful?
What can we do to improve the information ?