Technical FAQs

Ask a Question

What is the Schneider Electric part number for the "wiring arms" used on the 140DAI543 00 and 140DAO842 10 ?

The part number for the "wiring arms" or "Field Wiring Connectors"  as we refer to them is 140XTS002 00.
This connector is used on all Quantum discrete IO modules supporting up to 32 IO points.
It's also used on all of Quantum Analog IO


Issue: part number


Product Line: Quantum 140DAO842 10


Environment: n/a


Cause: n/a


Resolution: n/a

 
Was this helpful?
What can we do to improve the information ?