Technical FAQs

Ask a Question

Unity Pro V8.0: The "Unity Pro PlantStructure DTM library" is not updated after UnityPro_V80_HF_DTM Hotfix installation.

The "Unity Pro PlantStructure DTM library" version is 2.0.9 on Unity pro 8.0 without the HotFix installed. It should be updated to version 2.3.4 after installation of this Hotfix.
The version is displayed in the Windows Control panel in the Add/remove Program (or Programs and functionalities on Windows 7)
The installation of UnityPro_V80_HF_DTM Hotfix , downloaded on schneider-electric.com, shopping kiosk and Schneider Electric Software Update before 3 September 2014 can have this wrong behaviour on some PCs.
Installation of UnityPro_V80_HF_DTM Hotfix delivered since September 3rd, 2014 fixes this issue.
 
How to get the "Unity Pro PlantStructure DTM library" updated to the version 2.3.4 :
You have to re-install the new Hotfix version. You need before to unregister the previous version of the Hotfix launching attached reg file, the one for your Unity Pro Package XL, L or S.
 
And relaunch the installation of the Hotfix.
Was this helpful?
What can we do to improve the information ?