Technical FAQs

Ask a Question

Are the 140NOE77110 and the 140NOE77111 HOT swappable?

Title

Are the 140NOE77110 and the 140NOE77111 HOT swappable?

Issue
 
Product Line


Modicon Quantum

Environment
 
Cause

Resolution

The 140NOE77110 and the 140NOE77111 are HOT swappable. It is recommended that the project configuration be changed and downloaded to the processor, but if the CPU cannot be stopped it is not necessary. When there is a shutdown, you could load the configuration then.

Was this helpful?
What can we do to improve the information ?