Technical FAQs

Ask a Question

How do I import a Twidosuite .txt program file?

Title

How do I import a Twidosuite .txt program file?

Issue
 
Product Line

Twido Twidosuite

Environment
 
Cause

Resolution

To import a .txt program file into Twidosuite, you first need to startup Twidosuite, go into Programming mode and Create a New Project. Once you have the new project started you will need to go into the Program section where you would insert your logic. At the bottom right hand side of the screen there is an Import Program button. Select the import button and you will be prompted to open the .txt file.

Was this helpful?
What can we do to improve the information ?