Technical FAQs

Ask a Question

How do I get to the Segment Scheduler in Proworx 32?

Title

How do I get to the Segment Scheduler in Proworx 32?

Issue
 
Product Line

Proworx 32

Environment
 
Cause

Resolution

To get to the Segment Scheduler in Proworx 32 you will need to navigate to the Logic screen. To get to the Logic screen you can double click on Logic in the Project Navigation tree or select Logic from the Project toolbar. Once in the Logic screen the Network Navigator should be on the left hand side, if not right-click on the middle of the logic screen and select Navigation Tree. The Network Navigator should appear.


Right-click in the Network Navigator and select Segment Scheduler.





 

Was this helpful?
What can we do to improve the information ?