Technical FAQs

Ask a Question

How can one monitor an ATV61/71 drive over modbus if the drive is in HMI(local) keypad mode or terminal mode by switching F4 key?

Issue:
How can one monitor an ATV61/71  drive over modbus if the drive is in HMI(local) keypad mode or terminal mode by switching F4 key?

Product Line:
Altivar ATV61/71 using modbus network

Environment:
All

Cause:
Needs to know over the network when the drive is local keypad mode after pushing the F4 function key.

Resolution:
Address 8441 bit 2 will give you Graphics  display reference control.
Address 8442 bit 2 will give you Graphics display command control.
Was this helpful?
What can we do to improve the information ?