Technical FAQs

Ask a Question

Can I use my finger for the touchscreen input instead of the stylus on the Magelis XBTGH2460?

 
Issue:
Can I use my finger for the touchscreen input instead of the stylus on the Magelis XBTGH2460?
 
Product Line:
 
 
Environment:
 
 
Cause:
 
 
Resolution:
Yes, you can use your finger as touch input on the Magelis XBTGH2460.
Was this helpful?
What can we do to improve the information ?