Technical FAQs

Ask a Question

Is there a cable for the HMISTU and/or HMISTO that will allow separation of the screen and back module?

Title

Is there a cable for the HMISTU and/or HMISTO that will allow separation of the screen and back module?

Issue
 
Product Line

HMISTU, HMISTO

Environment
 
Cause

Resolution

There is a 3m cable that can be used to separate the HMI screen from the back module of the HMISTU's and HMISTO's. The part number for the cable is HMIZSURDP.

Was this helpful?
What can we do to improve the information ?