Technical FAQs

Ask a Question

Is there a remote cable available for the Magelis HMIS5T and HMISCU available?

For HMIS5T (base):

New products will come with a PV07 and a SV5.0 (end of october 2014) and they will be compatible with the remote cable (3m, 5m and 10m).
 

For HMISCU:

New products will come with a PV04 and a SV3.0 (end of october 2014) and they will be compatible with the remote cable (3m, 5m and 10m).


The part number for the cable will be HMIZSURDP*
* = Length available in 3m, 5m and 10m


Note: For old products, you will need to update them with VJD V6.2 SP2 (end of November 2014) in order to be use the remote cable.

 

 

Was this helpful?
What can we do to improve the information ?