Technical FAQs

Ask a Question

Why does Unity Pro v7.0 shut down when I am trying to print?

Title
Unity Pro v7.0 shuts down when trying to print.
Issue
Unity Pro v7.0 shuts down when trying to print a section of your Unity Pro v7.0 program.
Product Line
Unity Pro - Socollaborative Software

Environment
Windows 7 Operating System
Cause
Unity Pro v7.0 shuts down when trying to print when Microsoft Office 2007 or 2010 resides on the PC and the operating system is Windows 7.
Resolution
This is a known issue in Unity Pro v7.0 and has been corrected in Unity Pro v8.0. If you are unable to upgrade to Unity Pro v8.0 or remove Microsoft Office, email your project to Technical Support.  Technical Support will print your project as a pdf.
Was this helpful?
What can we do to improve the information ?