Technical FAQs

Ask a Question

Why is the Magelis XBTRT511 is not giving me the correct floating point value reading on the alphanumeric display when communicating with a Momentum?

If you address the alphanumeric display as a %MW that is incorrect.  To read a floating point value, you need to address the alphanumeric as a %MF.
Was this helpful?
What can we do to improve the information ?