Technical FAQs

Ask a Question

Can you set up XBTL1000 to display the input range from the numeric entry keypad of a alphanumeric object?

No, there is no option in the alphanumeric object settings of XBTL1000 to display the input range on the numeric entry keypad.
Was this helpful?
What can we do to improve the information ?