Technical FAQs

Ask a Question

What would cause a fault light on a 140CRA93100?

The fault light on the CRA module indicates that the card is not seeing one or more of the IO modules configured for the drop. It could be that a module is in the wrong slot/missing all together or that it has failed. If the IO module is in the backplane and is healthy and recognized, the word "Active" should appear at the top of the module. If none of the IO modules are "Active" it could be that the address switches at the back of the CRA are not properly set for that drop location. If all modules have the word 'Active', it could be that the Power Supply model number that is in the slot does not match the one in the configuration.





 
Was this helpful?
What can we do to improve the information ?