Technical FAQs

Ask a Question

What is the variable tag limit on a Magelis iPC?

Issue:
What is the variable tag limit on a Magelis iPC?

Product Line:
iPC, PC runtime

Environment:


Cause:


Resolution:

In Vijeo Designer v6.2, the Magelis iPCs could have up to 12000 variables per target.
Was this helpful?
What can we do to improve the information ?