Technical FAQs

Ask a Question

Error Restoring SQL2000 database backup on SQL Server 2012

Issue:
The database was backed up on a server running version 8.00.0760. That version is incompatible with this server, which is running version 11.00.3128.

Product  Line:
SQL Server 2000
SQL Server 2012

Environment:
SQL Server Database Restoration

Cause:
It is not possible to restore a SQL Server 2000 database on SQL Server 2012.

Resolution:
You will need to restore the database on an instance of SQL Server 2005, 2008 or 2008 R2 first, then back it up from there, then restore the new backup on SQL Server 2012.



Was this helpful?
What can we do to improve the information ?