Technical FAQs

Ask a Question

Does the M340 thermocouple BMXART0414 provide cold-junction compensation built-in to the card?

No. The preferred method to attain cold-junction compensation on the BMXART0414 is to use the ABE-7CPA412 Telefast block and set the channel configuration for External PT100.
Was this helpful?
What can we do to improve the information ?