Technical FAQs

Ask a Question

Can I use S-Box target with Vijeo Designer BT 6.2 ?

The Version of Vijeo Designer Build Time V6.2 contains 2 S-Box lines in the target list:

  • S-BOX PC Optimized HMIBSOxxxxxxx
  • S-BOX PC Universal HMIBSUxxxxxxx

They should not be present in this list and MUST NOT be used.

This issue will be fixed within the new service pack 6.2SP2 available on October 2014.

Was this helpful?
What can we do to improve the information ?