Technical FAQs

Ask a Question

What is the pin assignment of the RS485 port (COM2) of Magelis XBTGT6330?

The pin assignment if the RJ45 RS485 port, COM2, on Magelis XBTGT6330 is as follows.

1 - Not connected
2 - Not connected
3 - Not conected
4 - D1 output/input , Transfer data RS485
5 - D2 output/input , Transfer data RS485
6 - RTS , output , Request to send
7 - Not connected
8 - SG , Signal ground

See attached file for more details.


Was this helpful?
What can we do to improve the information ?