Technical FAQs

Ask a Question

Can I mix a Quantum 140CPU53414A with a 140CPU53414B in the same Hot Standby System?

No. The Quantum hardware models must match in a Quantum Hot Standby System. A Hot Standby System must have two 140CPU53414A or two 140CPU53414B CPU modules.
Was this helpful?
What can we do to improve the information ?