Technical FAQs

Ask a Question

What is the part number for the backlight replacement bulb of a XBTGT series HMI?

The backlight on the Magelis XBTGT can be replaced on certain model.

Model Catalog number
XBTGT5230 XBTZG43
XBTGT53*0 XBTZG45
XBTGT53*0 PV03 or greater / XBTRGT54*0 XBTZG45B
XBTGT63*0 XBTZG46
XBTGT7340 XBTZG47
Was this helpful?
What can we do to improve the information ?