Technical FAQs

Ask a Question

Do the M580 PLCs support the AUX tasks?

Issue NA
Product Line M580
Environment NA
Cause NA
Resolution Yes. The M580 PLCs support AUX tasks.
Was this helpful?
What can we do to improve the information ?