Technical FAQs

Ask a Question

Update firmware option in VAMPset is not available

Issue: Update firmware option in VAMPset is not available

Resolution: In order to update the firmware do not Connect to the Device. For a firmware update only configure the communication settings, do not click Connect Device. Once you have the communciations settings configured the update firmware option will be available.
Was this helpful?
What can we do to improve the information ?