Technical FAQs

Ask a Question

How to set the date/time for MiCOM protection relays from within MiCOM S1 Studio

Issue: Need to configure the date/time for the MiCOM relays

Resolution:
1. Connect to the MiCOM relay using MiCOM S1 Studio
2. Right click on the device
3. Select Supervise Device
4. Select Date/Time
5. You may set the date/time manually by entering the date/time or you may click Set Current Date/Time. This method will load the PC time into the MiCOM protection relay.
Was this helpful?
What can we do to improve the information ?