Technical FAQs

Ask a Question

Why is Proworx 32 looking for a .mdb file and giving me error # 3024 when I open a .pwx project file?

Title

Why is Proworx 32 looking for a .mdb file and giving me error # 3024 when I open a .pwx project file?

Issue

Cannot open Proworx 32 .pwx project file
 
Product Line

Proworx 32

Environment
 
Cause

When a Proworx 32 .pwx project file name is changed in Windows Explorer rather than in Proworx you will get error #3024 when trying to open the project.




Resolution

To resolve the issue the project file name needs to be changed back to the original name. If the name is not known, the project can be opened in notepad to reveal the original file name. Change the file name back to the original name in Windows Explorer. Once the name is changed back, the project should open in Proworx.



 

Was this helpful?
What can we do to improve the information ?