Technical FAQs

Ask a Question

PES returns 'Failed to find valid license after running for extended amount of time.

Applicable to Product Range(s) : Web Designer


Goals and Symptoms
PES returns 'Failed to find valid license after running for extended amount of time.

Facts and Change
PES version 3.1, SP1

Causes and Fixes
If you shutdown the server (that has a valid license ) after it has been running for an extended amount of time and then try to restart it sometime later, it could return the error:

Failed to find a valid license.
No license available for a specific product functionality.
Feature=EUS_BAS_Server 3.00

To resolve the issue, reboot the PC.

Was this helpful?
What can we do to improve the information ?