Technical FAQs

Ask a Question

What is the fusing recommendation for the Magelis HMISCU?

We recommend using a slow-blow, 2A type T fuse.  Type T and Class refer to different characteristics.

Type T is a time-delay slow blowing fuse.  They are available in a wide variety of form factors and amperages.  They typically have a fast over current link for surge spikes and a slower over current link for longer overload conditions.

 

Was this helpful?
What can we do to improve the information ?