Technical FAQs

Ask a Question

What are the diameters of the power and encoder cables for Lexium 32 drives?

The motor and power cable diameters for Lexium 32 drives can be seen in the file that is attached to this FAQ.

Was this helpful?
What can we do to improve the information ?