Technical FAQs

Ask a Question

What os the replacement for the Berger Lahr D065 motor with ID number 18001100015 ?

For Berger Lahr D065 motors that have ID number 18001100015 use the replacement part number of 18001200015, which is a N065 type motor.
The N065 will directly replace the D065.
 
Was this helpful?
What can we do to improve the information ?