Technical FAQs

Ask a Question

How do you set the IP Address on a Unity Quantum NOE?

Title

How do you set the IP Address on a Unity Quantum NOE?

Issue
 
Product Line

Unity Pro, Quantum

Environment
 
Cause

Resolution

To set the IP Address to a Quantum NOE, a new network needs to be setup. Within the Ethernet network configuration the appropriate Model Family needs to be selected. There are three Model Families to choose from that can be used for NOE's. Select the appropriate Model Family for the application. If you hover over the different model family options with your mouse you will see what each option covers as far as CPU's and NOE's.



Once the correct model family has been selected, the new network has to be linked to the NOE. To link the network select the Ethernet port on the NOE from the Project Browser. The NOE Configuration screen will come up. On that screen you will link the network previously setup, as seen below.

 
Was this helpful?
What can we do to improve the information ?