Technical FAQs

Ask a Question

What is the purpose of No. of Records in RAM in Vijeo Designer?

No. of Records in RAM is the quantity of records to be kept in SRAM before the log data is flushed to a file.  File could be either Secondary (CF card) or Optional (USB Flash Drive)  depending on the setting in data location.
Was this helpful?
What can we do to improve the information ?