Technical FAQs

Ask a Question

In Vijeo Designer 6.2 If I use the set bit function in an Action how long will the bit stay on?

The bit must be reset by an Action or other function in the Vijeo Designer program. It will also reset if the HMI is power cycled and you do not have the retentive property set to enabled for the variable you are setting with the action.
Was this helpful?
What can we do to improve the information ?