Technical FAQs

Ask a Question

What does the STATUS light on the TwidoPort indicate?

Issue:
Flashing STATUS light on the TwidoPort



Product Line:
Twido




Environment:





Cause:





Resolution:
This table describes the condition(s), and blink patterns of the STATUS LED on the module:

STATUS (green)
on = normal condition
off = abnormal condition
blink 2 = invalid MAC address
blink 3 = link not connected
blink 4 = duplicate IP connection
blink 5 = attempting to get IP condition through BootP
blink 6 = default IP condition

 

Was this helpful?
What can we do to improve the information ?