Technical FAQs

Ask a Question

Unable to subscribe to GOOSE messages using a Vamp 200 series protection relay

Issue: GOOSE inputs are not selectable from the ICD file created from a VAMP 200 series relay with GOOSE subscrption enabled.

Product Line: Vamp 200 series

Resolution: When creating the ICD file from a connected VAMP 200 series relay you much select the SCL generation option "Edition 2 extensions." This will allow you to subscribe to GOOSE messages.
Was this helpful?
What can we do to improve the information ?