Technical FAQs

Ask a Question

What material are the braking resistors made of?

Issue:
What material are the braking resistors made of?
Product Line:
VW3A7803  VW3A7804
Environment:
All VW3A7803  VW3A7804
Cause:
N/A

Resolution:
The braking resistors are composed of the following materials:

Stainless steel
Extracts of natural rock
Magnesium silicate
Alumina oxides
Aluminum

 
Was this helpful?
What can we do to improve the information ?