Technical FAQs

Ask a Question

How do you set the IP Address on a Unity Quantum PLC?

Title

How do you set the IP Address on a Unity Quantum PLC?

Issue
 
Product Line

Unity Pro, Quantum

Environment
 
Cause

Resolution

To set the IP Address to a Quantum CPU, a new network needs to be setup. Within the Ethernet network configuration the appropriate Model Family needs to be selected. The default Ethernet model family is set to Regular Connection. The model family needs to be set to Extended Connection for a CPU. If you hover over the different model family options with your mouse you will see what each option covers as far as CPU's and NOE's.




Once the correct model family has been selected, the new network has to be linked to the CPU. To link the network select the Ethernet port on the CPU from the Project Browser. The CPU Ethernet Configuration screen will come up. On that screen you will link the network previously setup, as seen below.

Was this helpful?
What can we do to improve the information ?