Technical FAQs

Ask a Question

Can the HMISTU655/855 be configured for the RS422/485 port in Vijeo Designer v6.1 with the Mitsubishi FX3U PLC?

Title

 Can the HMISTU655/855 be configured for the RS422/485 port in Vijeo Designer v6.1 with the Mitsubishi FX3U PLC?

Issue

xxxxxx
 

Product Line

Vijeo Designer
 

Environment

xxxxxxx
 

Cause

xxxxxxx
 

Resolution

No. Currently there is no driver designed to communicate directly without a converter. An RS232 to an RS422/485 converter must be implemented.

Was this helpful?
What can we do to improve the information ?