Technical FAQs

Ask a Question

Do the internal %M coils maintain last state during an M340 power cycle?

Issue
 N/A
 
Product Line
 M340

Environment
 
NA
 
Cause
NA
 
Resolution
By default the %M coils do maintain last state during a power cycle. As of firmware version 2.40 this behavior is selectable under Project Settings -> PLC behaviour.



 
Was this helpful?
What can we do to improve the information ?