Technical FAQs

Ask a Question

How do I connect to a XBTN200/400 with a Magelis Logo?

To connect to a Magelis XBTN200/400 with a Magelis Logo you need the following:

TSXCUSB485 (USB to RS485 adapter. Rotary switch set to 0 TER Multi. Polarization On.)
XBTZN999 (RJ45 to RJ45)*
XBTZ925(A) (1 side connected to XBTXN999 side, 2 connected to Magelis side.

You can also make your own cable (This pinout only works with XBTN200/400 with Magelis logo)
RJ45 Male (TSXCUSB485 side) to RJ45 Male (Magelis Side)
5 to 4
4 to 5
7 to 7
8 to 8
8 and 1 jumped on Magelis side
6 and 8 jumped on TSXCUSB485

*XBTZN999 is not required for the XBTN200/400 with the Telemecanique logo.

Was this helpful?
What can we do to improve the information ?