Technical FAQs

Ask a Question

What is the replacement for a VRDM3913/50LWB motor bearing part number 52127035600?

Issue: The VRDM 3xxx stepper motors have been replaced with a new product reference.

Product Line:
VRDM Stepper Motors. BRS Stepper motors


Cause: VRDM 3xxx motors are not sold with a new reference part number and hence not available on the System with the older product reference.

Resolution :

The VRDM motor bearing part number 52127035600 had the following type code.

VRDM3913/50LWB 00IP41 00 D4E 73 0000000. These motors have since bene replaced by the BRS product reference.
The corresponding BRS motor for the above VRDM reference is BRS39BWE70ABA.

Was this helpful?
What can we do to improve the information ?