Technical FAQs

Ask a Question

What is the raw data resolution of the 140ACO02000 analog output module?

Title
 Quantum analog output card data resolution.
 
Issue
Output card specifications.
Product Line
Modicon Quantum
Environment
 
NA
Cause
 NA
 
Resolution
The 140ACO02000 is a 12 bit module and the raw data range is 0-4095.

 
Was this helpful?
What can we do to improve the information ?