Technical FAQs

Ask a Question

What's the difference between Magelis XBTN401(1) and XBTN401(2) in XBTL1000 or Vijeo Designer Lite?

 Issue:
What's the difference between Magelis XBTN401(1) and XBTN401(2) in XBTL1000 or Vijeo Designer Lite?
 
Product Line:
Magelis XBTN401, XBTL1000, Vijeo Designer Lite
 
Environment:
 
 
Cause:
 
 
Resolution:
When selecting the terminal type for the XBTN there are 2 selections. 
The XBTN401(1) has the functions keys predefined for F1-F4 and can be configured.
The XBTN401(2) when selected the function keys are predefined for "DEL" , Up Arrow , Down Arrow , and "MOD" 

If you want to write a numeric value to a register in the PLC, you need to select the XBTN401(2).  The XBTN401(1) is a read only target.
Was this helpful?
What can we do to improve the information ?