Technical FAQs

Ask a Question

Can the Advantys Reflex Action function blocks configured in a NIM (Network Interface Module) be animated when online with the configuration software ?

Title

Can the Advantys Reflex Action function blocks configured in a NIM (Network Interface Module) be animated when online with the configuration software ?

Issue

 

Product Line

Advantys STB

Environment

 

Cause

 

Resolution
 

No, the reflex actions cannot be animated when online with the Advantys configuration software.

Was this helpful?
What can we do to improve the information ?