Technical FAQs

Ask a Question

Is the Ethernet connection on the M1E controllers and ENT communication adapters 10baseT or 100baseT?

Title

Is the Ethernet connection on the M1E controllers and ENT communication adapters 10baseT or 100baseT?

Issue

 

Product Line

Modicon Momentum

Environment

 

Cause

 

Resolution

The speed of the Ethernet connection on all M1E controllers and ENT communication adapters is 10 base T half duplex, except the 171CBB97030 processor with embedded switch and the 170 ENT 110 01 I/O base communication adapter which are 10/100 base T half/full duplex.

Was this helpful?
What can we do to improve the information ?