Technical FAQs

Ask a Question

Do the 115 VAC isolated Input and Output Advantys STB modules require a dedicated or special PDM module?

Title

Do the 115 VAC isolated Input and Output Advantys STB modules require a dedicated or special PDM module?

Issue

 

Product Line

Advantys STB

Environment

 

Cause

 

Resolution

No, any 115 VAC PDM can be used. These modules (STBDAI5260 and STBDAO5260) are isolated and do not receive power from the PDM. Therefore, two different sources or phases can be wired to each input or output.

Was this helpful?
What can we do to improve the information ?