Technical FAQs

Ask a Question

Are there any high density discrete modules available for Advantys STB?

Title

Are there any high density discrete modules available for Advantys STB?

Issue

 

Product Line

 

Environment

 

Cause

 

Resolution

Yes there are two Advantys high density discrete modules available.

The STBDDI3725 is a 16 point, 24 Vdc, true high, sink digital input module.

The STBDDO3705 is a 16 point, 24 Vdc, true high, source, digital output module.

Each module requires two 18-point terminal connectors.
The STBXTS1180 is a set of two 18-point I/O screw type connector.
The STBXTS2180 is a set of two 18-point I/O spring type connector.
Each set of connectors has to be ordered separately.
These modules will auto-configure into the system without the use of the configuration software. To access the Help Screens and view or modify the configuration, minimum version 2.0 of the Advantys configuration software (STBSPU1000) will be required.

Was this helpful?
What can we do to improve the information ?