Technical FAQs

Ask a Question

What condition may bring about stop code 0400 on a Unity Quantum CPU

Title

What might cause stop code 0400


Issue




Product Line

Unity Quantum CPU's


Environment

n/a


Cause

n/a



Resolution

 Stop code 0400 can occur if you download a Unity file with "Change Configuration on the Fly" or CCOTF  selected but the
 CRP9 in the PLC back plane is using firmware <2.0 . The CCOTF option was offered with CRP9 firmware version =>2.0 .
 If you experience the 0400 stop state check the PLC configuration for a selection of CCOTF and disable this functionality.
 You could also re-flash the CRP9 with a firmware version that supports CCOTF.

 
Was this helpful?
What can we do to improve the information ?