Technical FAQs

Ask a Question

What are the cut-out dimension for the Magelis Panel PCs?

The correct cut-out dimension for the Panel PCs are as follow:

15"  Panel: 383.5 X 282.5mm +1mm

19" Panel: 459.5 X 359.5mm +/-0.5mm
Was this helpful?
What can we do to improve the information ?